cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot recognize device when connected to STM32cubeprogrammer

MDeac.1
Associate III

I have set up the device, 5V 3A wall PSU and connected to the USB stlink connection. Connecting to the onboard stlink I can recognize the board serial number but the programmer fails to recognize the device. What am I missing? The device works perfectly in stand alone mode. As it would not identify the device I upgraded the firmware to V2J37M26 to see if that would correct it.

 

This was the output in the programmer if it helps.

 

12:26:58 : ST-LINK SN : 0669FF333536414257062332

 12:26:58 : ST-LINK FW : V2J37M26

 12:26:58 : Board    : --

 12:26:58 : Voltage   : 3.27V

 12:26:58 : SWD freq  : 4000 KHz

 12:26:58 : Connect mode: Normal

 12:26:58 : Reset mode : Hardware reset

 12:26:58 : Error: Cannot identify the device

1 ACCEPTED SOLUTION

Accepted Solutions
MDeac.1
Associate III

Okay by trying different things blindly the dip switches on the board enabled discovery of the device.

So problem solved.

View solution in original post

1 REPLY 1
MDeac.1
Associate III

Okay by trying different things blindly the dip switches on the board enabled discovery of the device.

So problem solved.