2024-03-07 05:18 PM
i've installed versions of STM32CubeProgrammer on my windows 10 PC as well as my MAC....
i'm following the instructions in um2269 (section 😎 on updating firmware, but see a message saying "No DFU detected" under the USB configuration panel.... selecting Connect fails at that point....
on windows, the device manager seems to identify a 'Power Shield (Virtual ComPort in FS Mode)' as well as a new 'USB Serial Device' when i plug in my board.... but there is a warning sign that ultmately tells me that windows can't find a driver.... drivers were definitely installed along with CubeProgrammer; and i've run some .bat file under the Drivers folder....
do i need to do anything with my (brand new) board??? if i move the sliding jumper to the 'Syst' position *BEFORE* plugging in the board, it doesn't even power up....
Solved! Go to Solution.
2024-03-08 01:57 PM
you really *DO* need to slide that jumper in the 'Syst' position before plugging in the board -- even if the board appears dead....
all's well after updating the firmware to the latest version....
2024-03-08 01:57 PM
you really *DO* need to slide that jumper in the 'Syst' position before plugging in the board -- even if the board appears dead....
all's well after updating the firmware to the latest version....