cancel
Showing results for 
Search instead for 
Did you mean: 

The 2.14 CubeProgrammer is slower than the 2.8 programming speed

xelus
Associate

Hi, I was using CubeProgrammer version 2.8 to program the STM32L552 microcontroller, using the ‘STM32_Programmer_CLI’ file. After updating to version 2.14, I have noticed a significantly longer programming time. For example, before the update, it took 1.8 seconds to program approximately 20kB; after the update, it takes over 10 seconds. My programming settings are as follows:
call "%programmer%" -c port=swd freq=1000 -w "%hexfile%" -v

I have tried different SWD frequencies, 3300 and 24000, but no luck. Does anyone else have this issue and know the solution?

I also have one more question - if a verification error occurs, why does STM32_Programmer_CLI return 0 as the exit code? Shouldn’t it be a different value that indicates an error?
Best regards,

 

22 REPLIES 22

Hi @kweenie 

Thank you for the quick test. I was really hoping that would help with the programming time, but that would have been too simple, haven't it ?

Regarding the write protection address, it could be a real fix that has been made after v13, the only way to know is to look at the device datasheet, which is / should be the ultimate truth.

I replaced the '425' files (html or stdlr) from v13 into the corresponding v18 folders for these folders:

  • C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\api\Data_Base
  • C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\api\lib\FlashLoader
  • C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\FastROM_Data_Base
  • C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\FlashLoader
  • C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Data_Base

AND..... bham, back at 2s ???

 

 

and now ?

who can 'forward' this to ST ?

Excellent, kudos for digging deeper and getting it to work !

Then again, why should it need the files scattered in 5 different places ?

@Aziz BRIGUI

Hi Aziz,

did you notice this thread ?

Just to inform you that also v2.19 flashes the '425' chip (ID 425, STMicroelectronics, Cortex-M0+, STM32L03x/L04x/L010, ARM 32-bit Cortex-M0+) 10x slower than previous versions ?!
I think this was broken in v2.12...

Any comments on the STM side ?

@Aziz BRIGUI 

Aziz (or anyone else), 

how/where can I open a support request for this (since you are not reacting) ?

Hello @kweenie,

Thanks for bringing this to our attention.

We are already investigating the concerns you raised internally (Internal tracking number: 205049).

Please be patient, I will get back to you ASAP.

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Aziz,

no news ?

@Aziz BRIGUI 

Aziz ??

Hello @kweenie & All,

I apologize for the late reply, as you might suspect addressing all what has been discussed in this thread with proper analysis can take some time.

1- Let me address the first point on STM32L552 (0x472):

I confirm there was a regression in performance in v2.14, however, this has been already fixed for that device in the recent releases, below you'll find the detailed benchmark:

HW used: STM32L562-DK, BL.bin is a 26 KB binary.
PS C:\Users\briguiah> Measure-Command {& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer 2.8\bin\STM32_Programmer_CLI.exe" -c port=SWD -d "C:\Users\briguiah\OneDrive - STMicroelectronics\Desktop\Projects\PRG_Projects\binaries\BL.bin" 0x08000000}


Days              : 0
Hours             : 0
Minutes           : 0
Seconds           : 0
Milliseconds      : 950
Ticks             : 9504560
TotalDays         : 1.10006481481481E-05
TotalHours        : 0.000264015555555556
TotalMinutes      : 0.0158409333333333
TotalSeconds      : 0.950456
TotalMilliseconds : 950.456



PS C:\Users\briguiah> Measure-Command {& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer 2.14\bin\STM32_Programmer_CLI.exe" -c port=SWD -d "C:\Users\briguiah\OneDrive - STMicroelectronics\Desktop\Projects\PRG_Projects\binaries\BL.bin" 0x08000000}


Days              : 0
Hours             : 0
Minutes           : 0
Seconds           : 3
Milliseconds      : 228
Ticks             : 32284463
TotalDays         : 3.73662766203704E-05
TotalHours        : 0.000896790638888889
TotalMinutes      : 0.0538074383333333
TotalSeconds      : 3.2284463
TotalMilliseconds : 3228.4463



PS C:\Users\briguiah> Measure-Command {& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer v2.19 S\bin\STM32_Programmer_CLI.exe" -c port=SWD -d "C:\Users\briguiah\OneDrive - STMicroelectronics\Desktop\Projects\PRG_Projects\binaries\BL.bin" 0x08000000}


Days              : 0
Hours             : 0
Minutes           : 0
Seconds           : 0
Milliseconds      : 902
Ticks             : 9027665
TotalDays         : 1.04486863425926E-05
TotalHours        : 0.000250768472222222
TotalMinutes      : 0.0150461083333333
TotalSeconds      : 0.9027665
TotalMilliseconds : 902.7665

 As you can see, best programming performance is with the latest version of STM32CubeProgrammer (v2.19).

2- For the 0x425 (STM32L03x/L04x/L010):

I confirm the 10x performance regression. Regression happened in v2.15 and is STRICTLY a Flashloader issue => The correct workaround is to only replace 0x425.stldr from v2.14 to v2.19 (I've attached the loader for convenience, it needs to be replaced in "STM32Cube\STM32CubeProgrammer\bin\FlashLoader").

Below the detailed benchmark:

HW used: Nucleo-L031, BL.bin is a 26 KB binary.
PS C:\Users\briguiah> Measure-Command {& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer 2.15\bin\STM32_Programmer_CLI.exe" -c port=SWD -d "C:\Users\briguiah\OneDrive - STMicroelectronics\Desktop\Projects\PRG_Projects\binaries\BL.bin" 0x08000000}


Days              : 0
Hours             : 0
Minutes           : 0
Seconds           : 24
Milliseconds      : 171
Ticks             : 241714877
TotalDays         : 0.00027976258912037
TotalHours        : 0.00671430213888889
TotalMinutes      : 0.402858128333333
TotalSeconds      : 24.1714877
TotalMilliseconds : 24171.4877



PS C:\Users\briguiah> Measure-Command {& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer 2.14\bin\STM32_Programmer_CLI.exe" -c port=SWD -d "C:\Users\briguiah\OneDrive - STMicroelectronics\Desktop\Projects\PRG_Projects\binaries\BL.bin" 0x08000000}


Days              : 0
Hours             : 0
Minutes           : 0
Seconds           : 2
Milliseconds      : 518
Ticks             : 25182709
TotalDays         : 2.91466539351852E-05
TotalHours        : 0.000699519694444444
TotalMinutes      : 0.0419711816666667
TotalSeconds      : 2.5182709
TotalMilliseconds : 2518.2709

I can assure you our Flashloader team is working hard to investigate further and fix this issue for a future release.

3- @Kraal, to address your enquiry on why the tools needs the files scattered in 5 places:

It's 2 different places actually (CubeProgrammer base path & CubeProgrammer API path). This is done because customers will not develop their CubeProgrammer based application inside the CubeProgrammer installation path => For customer convenience, copying only the API path should work out of the box, that brings the need for bundling Flashloader and Database in the API folder.

PS: FastROM_Data_Base is not the same as the database in base path (It's needed for a specific purpose which is the ST FastROM procedure).

I've tried to address as many points as I could, please let me know via PM or comment if any points where missed.

Thanks for your efforts in pre-analyzing these issues.

Aziz

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.