cancel
Showing results for 
Search instead for 
Did you mean: 

Thanks for Incremental Flash

codebuk
Associate III

Hi,

Many thanks for the experimental incremental flash feature! For me it speeds up the dev cycle considerably.  

(Note https://wiki.st.com/stm32mcu/wiki/STM32CubeProgrammer_errata_2.21.x seems to be broken.)

Dan

 

1 ACCEPTED SOLUTION

Accepted Solutions
mfgkw
Senior III

Maybe this is related to another bug: STM32CubeProgrammer is not available yet :)

The downloads only show up to 2.20.0

(Or ST recalled 2.21 for some reason)

 

https://www.st.com/en/development-tools/stm32cubeprog.html

View solution in original post

2 REPLIES 2
mfgkw
Senior III

Maybe this is related to another bug: STM32CubeProgrammer is not available yet :)

The downloads only show up to 2.20.0

(Or ST recalled 2.21 for some reason)

 

https://www.st.com/en/development-tools/stm32cubeprog.html

Hi,

This thread is to say thanks and to note that the speed of the code-flash-test cycle especially when a lot of flash is in use is very important to me.

Thanks again.

Dan