2024-05-16 7:06 AM - edited 2024-05-16 8:23 AM
Hello,
I have developed a external Loader for my custom projekt. It uses a W25Q128 QSPI conected to bank 2 and alternative Pin of CLK. (Worse!, but it is so...) So i Have no exactly example for it. Also it is a Dual Core, and no example i find have special definitions for it.
I worked more days on it and it worked perfekt (now!) in a Cube Projekt.
Erase, write and read (manual) and memory mapped mode are perfect.
If I compile the stldr file, I can load ist in Cube programmer and stm prog utility.
But then I could cry. I can't do anything. No read on QSPI and so on.
....
I think i will have trouble with the m4 Core. The M7 Core must wait for him.
I don't know. How you can help me. What is wrong. Have you any Idea?
2026-01-19 12:31 AM
No, ask Tesla DeLorean