2022-01-25 2:26 PM
I tried to connect the STLink to the STM32G030K6T6 by connecting SWCLK SWDIO VDD and GND pins, but the STM32CubeProgrammer can't detect the MCU.
I also tried to check with the logic analizer the pins and there is only a little signal from the stlink but no response from the MCU.
I think the problem could be that the SWCLK and BOOT0 are in the same pin and this is pulled down internally. So how can I connect and program the STM32?
Thank you so much
Solved! Go to Solution.
2022-01-25 4:50 PM
Okay I resolved by updating the STLink. Now it works. Thank you
2022-01-25 3:23 PM
Is this chip powered? (ST-Link does not provide power)
Is this a custom board or known good hardware?
Is NRST high? Voltage levels okay? What is this history of the chip?
2022-01-25 4:50 PM
Okay I resolved by updating the STLink. Now it works. Thank you
2022-04-08 8:24 AM
I've the same problem but I'm using the ST-Link of the nucleo board, my version is V2.J39.S0. Any idea?
Thanks.