cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer update

MSand.1
Associate II

Hi,

 

I am using STM32CubeProgrammer 2.4 version on a PC (let me call it PC_1, Windows 11 Enterprise OS) for programming a board (a customized seld-developped one) where there is also the STM32CubeIDE SW for FW development. You see below the program screen

MSand1_0-1721902597386.jpeg

 

On a second PC (let me call it PC_2, Windows 10 Enterprise OS) I installed STM32CubeProgrammer 2.16 version:

in this case I am not able to connect (for programming) the same board (with the same ST-LINK V2 device and cable) I am able to program on PC_1 with STM32CubeProgrammerr 2.4. You see below the PC screen:

MSand1_1-1721903062092.jpeg

NO STM32 target is found!!

Note that before making the connection, by clicking on the left  button on Serial Number row the program is able:

to detect the presence/absence of the STLINK device;

to detect the target voltage (when powered on/off)

but the connect operation does not work.

 

How can I solve this problem? 

 

Thank in advance for your help

 

Mario

1 REPLY 1
Aziz BRIGUI
ST Employee

Hello @MSand.1,

I apologize for the late reply,

Could you try using  CubeProgrammer v2.17 and get back to us with the results ? We are not able to reproduce on our side.

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.