cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer update

MSand.1
Associate II

Hi,

 

I am using STM32CubeProgrammer 2.4 version on a PC (let me call it PC_1, Windows 11 Enterprise OS) for programming a board (a customized seld-developped one) where there is also the STM32CubeIDE SW for FW development. You see below the program screen

MSand1_0-1721902597386.jpeg

 

On a second PC (let me call it PC_2, Windows 10 Enterprise OS) I installed STM32CubeProgrammer 2.16 version:

in this case I am not able to connect (for programming) the same board (with the same ST-LINK V2 device and cable) I am able to program on PC_1 with STM32CubeProgrammerr 2.4. You see below the PC screen:

MSand1_1-1721903062092.jpeg

NO STM32 target is found!!

Note that before making the connection, by clicking on the left  button on Serial Number row the program is able:

to detect the presence/absence of the STLINK device;

to detect the target voltage (when powered on/off)

but the connect operation does not work.

 

How can I solve this problem? 

 

Thank in advance for your help

 

Mario

0 REPLIES 0