cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer (2.7.0) screen get corrupted. Any ideas ?

ESore.2
Associate

After PC boot program works fine for some time but after some time the screen is corrupted.

(also seen a completely black or a completely white screen). When clicking the pop-up windows are however OK.

3 REPLIES 3
Imen.D
ST Employee

Hello @ESore.2​ and welcome to the Community :)

Please use the new release STM32CubeProgrammer 2.8.0 available in the ST web site.

Then, please keep me informed about your update.

If your issue is solved, please mark my answer as best by clicking on the "Select as Best" button. This will help other users find this solution more quickly.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hi @ESore.2​ ,

Please share your update and let me know if your issue is solved with latest release of CubeProgrammer.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
ESore.2
Associate

Finally I managed to update to version 2.8.0 - unfortunately the problem persists :|

I managed to see a message which was showed for a very short moment and only one time when trying to start the program

The message was something like "OpenJDP Platform binary not responding" and was in local language (so probably a windows generated message)

After a PC reboot the STM32CubeProgrammer 2.8.0  always start. If start fails it may restart after a number of retries.

In some cases it seems like the although the screen is blank, the program still reacts on mouse clicks.

Could the reason for the problem be that the OpenJDP Platform binary software does not work stable on my PC*

*) HP ProBook 470 with Intel HD Graphics 4600 / Windows 10