STM32CubeProgrammer 2.11.0 released
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-01 1:47 AM
New features
• Tool updater: can be used to upgrade STM32CubeProg from v2.10.0 to v2.11.0 for all supported operating systems (Windows®, Linux®, and macOS®)
• SFI: – SFIx support for STM32U585xx microcontrollers via SWD/JTAG – New SFI/SFIx graphical user interface (GUI) – STM32 Trusted Package Creator SFI GUI enhancement – Support for integrity check with the STM32H7 Series and STM32U5 Series microcontrollers • STM32U5 Series: the GUI supports the RDP regression with password
• New bootloader support for STM32L476xx microcontrollers
• STM32MP13xx microprocessors: – Flash memory load via USB-DFU/UART – SSP (command-line interface only) – OTP: CLI/GUI
Fixed issues
90858 [STM32WB][CLI] Optimize FUS, STACK, and USER app upgrading automatically. 104409 STM32H735xx: SFI is very slow over SWD.
109240 Extra option bytes displayed for STM32G030C6: PCROP1A_STRT, PCROP1A_END, PCROP1A_RDP, PCROP1B_STRT, PCROP1B_END, and BOOT_LOCK, SEC_SIZE.
110205 Fix the reading of CHIPID (DBGMCU_DBG_AUTH_DEVICE) on STM32U5 microcontrollers.
110614 [CLI] Error level not reported correctly for the CRC safety feature using STM32CubeProgrammer_CLI.
117163 Launch problem when running the STM32CubeProgrammer GUI from another path.
119604 [STM32G0][OB] Sector erase cannot be achieved and an STM32CubeIDE debug error occurs when nSWAP_BANK=0.
120935 STPC v2.9 cannot generate a correct .sfi file for SFI.
121452 [OB] Incorrect SRAM2b secure address for STM32WB1xxx.
121713 Typo: “Memory & file edition�?.
123018 [STM32H7][CM4] BOOT_CM4_ADD cannot be modified.
123740 [DFU] The single-bank configuration is not correctly managed when connecting with DFU.
123913 [CLI] It is not possible to write the LOCK byte.
123923 [UART] A timeout error occurs while disabling the readout protection.
124081 Odd behavior in the log when connecting a NUCLEO-F030R8 using the GUI.
124446 Request to add documentation for the getAuthID command.
124763 [OB] Wrong description of nBOOT1.
125039 [DFU] Strange behavior when trying to program in single-bank mode.
127099 [STM32L4+] Fail to program STM32L4+ twice in a row.
127311 The tool closes automatically when trying to load a file the path of which contains Chinese characters.
127978 Typo in option bytes: IWGDSTDBY.
- Labels:
-
STM32CubeProgrammer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-01 5:25 AM
https://www.st.com/en/development-tools/stm32cubeprog.html
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
‎2022-07-01 6:57 AM
In case anyone is wondering: there is unfortunately still a typo in the name in the URL (...-v2100-...), but it refers to the correct and current revision 20 of RN0109 for 2.11.0.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-01 7:05 AM
@Nawres GHARBI​ thank you to you and Programmer and Loaders team(s)..
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
‎2022-11-18 2:32 AM
I still have problems with the STM32 Programmer in DFU Mode! The programming is running through with a verify error and the controller still has the old programm? See LOG from the programmer!
11:29:32 : USB speed : Full Speed (12MBit/s)
11:29:32 : Manuf. ID : STMicroelectronics
11:29:32 : Product ID : STM32 DownLoad Firmware Update
11:29:32 : SN : 206130A74734
11:29:32 : DFU protocol: 1.1
11:29:32 : Board : --
11:29:32 : IAP
11:29:34 : UPLOADING ...
11:29:34 : Size : 1048576 Bytes
11:29:34 : Address : 0x8000000
11:29:34 : Read progress:
11:29:35 : Data read successfully
11:29:35 : Time elapsed during the read operation is: 00:00:02.450
11:29:47 : Memory Programming ...
11:29:47 : Opening and parsing file: STM32L476_DFU.hex
11:29:47 : File : STM32L476_DFU.hex
11:29:47 : Size : 106.77 KB
11:29:47 : Address : 0x08000000
11:29:47 : Erasing memory corresponding to segment 0:
11:29:47 : erasing sector 0000 @: 0x08000000 done
11:29:47 : erasing sector 0001 @: 0x08004000 done
11:29:47 : erasing sector 0002 @: 0x08008000 done
11:29:47 : erasing sector 0003 @: 0x0800c000 done
11:29:47 : erasing sector 0004 @: 0x08010000 done
11:29:47 : Download in Progress:
11:29:48 : File download complete
11:29:48 : Time elapsed during download operation: 00:00:00.481
11:29:48 : Verifying ...
11:29:48 : Read progress:
11:29:48 : Error: Data mismatch found at address 0x08000400 (byte = 0xB0 instead of 0xC0)
11:29:48 : Error: Download verification failed
11:29:48 : RUNNING Program ...
11:29:48 : Address: : 0x08000000
11:29:48 : Start operation achieved successfully
11:29:48 : Warning: Connection to USB device is lost
11:29:48 : Disconnected from device.