cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.1.0 won't launch on Mac running OS 10.13.6

KHill
Associate

Installed by way of the opening Package Contents method. When I double click to lunch STM32CubeProgrammer it does not run. Tried reinstalling, restarting. Running java 8 update 211

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @RChap.1​ ,

Thanks for your feedback,

Check my comment in this thread, it might help solving your issue.

Sara.

View solution in original post

4 REPLIES 4
DShel
Associate

Hi, did you ever get this solved? I have the same problem on OS 10.12.6

kind regards,

Damian

JPate.1950
Associate

Likewise - double clicking the installed app just bonces the icon in the dock once and then quits . You can get it to run by right clicking on the installed package (STM32CubeProgrammer.app), selecting 'Show package contents' and navigating to

Contents/MacOs/bin/STM32CubeProgrammer

and right clicking 'open'. I made an alias of this and put it in the top directory for easier access.

RChap.1
Associate

Can't run even on MacOS 12.6.3 with the above trick but there is a telltale error message in the command window:

"Exception in thread "AWT-EventQueue-0" com.izforge.izpack.api.exception.IzPackException: com.izforge.izpack.api.exception.ResourceNotFoundException: Image icon resource not available from url: jar:file:/Users/someguy/Downloads/en/SetupSTM32CubeProgrammer-2.12.0.exe!/resources/Splash.image"

Note the reference to the .exe file resource for the splash image. This is a Mac App. Somebody missed a dependancy link in the mac compile. And they must not have tried hard to test it as it is delivered broken.

Hello @RChap.1​ ,

Thanks for your feedback,

Check my comment in this thread, it might help solving your issue.

Sara.