2025-02-26 2:56 AM
If on a STM32H747 the Cortex-M4 (BCM4 or BOOT_M4 Bit) is disabled by software, it is impossible to reactivate it with the STM32CubeProg v2.18.0 because the checkbox disappears in the user interface. But this happens only if you do a power cycle and reconnect to the target.
Solved! Go to Solution.
2025-02-28 12:49 AM - edited 2025-02-28 12:49 AM
So it's a GUI issue not related to the hardware.
Internal ticket 204208 has been opened for analysis. This ticket is not accessible by the community users.
2025-03-05 1:51 AM - edited 2025-03-05 1:51 AM
Behavior reproduced internally by our teams.
It will be analyzed asap.
2025-05-06 11:00 AM
Any update on this? I have the exact same issue. I unchecked BCM4 in STM32CubeProgrammer for STM32H745, and then after reboot, the checkbox isn't even there to check it again.
Also, it is not just GUI because the Cube Programmer CLI says the BCM4 register isn't available now.
2025-05-06 11:48 AM
If there were any update I've already provided it..
Don't expect to have an updated version very soon. I will keep you informed for any update.
Thank you for your understanding.
2025-11-17 8:15 AM
Hello @dariis
Issue fixed in the latest STM32CubeProgrammer release available under this link: STM32CubeProg | Software - STMicroelectronics.
Aziz