2024-05-01 11:44 AM - edited 2024-05-02 12:18 AM
Hi 🙂
Problem: STM32F030R8T6 device not found.
ErrorMsg in CubeProgrammer: "No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication."
ErrorMsg in CubeIde: "Error in initializing ST-LINK device. Reason: No device found on target."
Setup: I made a breakout-board for an STM32F030R8T6. The board only carries the µC and spreads out the pins to use on a breadboard. I connected all VSS and VDD pins and used 0.1µF capacitors as close as possible to the µC. I connected the ST-Link-V2 as follows:
VSS -> any GND pin
VDD -> any 3V3 pin
NRST -> NRST (pin 7) (not sure if I need to connect the pin somehow aside from the debugger)
SWDIO -> SWDIO (pin 46) 220Ohm Pullup
SWCLK -> SWCLK (pin 49) 220Ohm Pulldown
I tried BOOT0 pin pulled low or high, both didn't work.
I double and tripple checked my connections. I am using the right pins on both sides and the µC has power.
-----------------------------------------------------------------
SOLUTION:
If you are NOT using an additional power supply you have to connect VDD and VAPP (pin 1 or 2 and pin 19 on STLinkV2) to the STM32's VDD.
VDD on STLinkV2 supplies power and VAPP senses target voltage. If the programmer can't sense a voltage you cannot connect.
So here is the correct configuration:
VSS -> any GND pin
VDD -> any 3V3 pin (to supply target with power)
VAPP -> any 3V3 pin (to sense target voltage)
SWDIO -> SWDIO (pin 46) no Pullup or Pulldown, leave pin floating
SWCLK -> SWCLK (pin 49) no Pullup or Pulldown, leave pin floating
I tried BOOT0 pin pulled low to use internal storage.
Depending on you application:
NRST -> NRST tied low through 100nF capacitor
Solved! Go to Solution.
2024-05-01 11:33 PM
Na, it has power now :
(But it should show 3V also in the blue panel, before "connect" . Hmmm...)
So with original st-link you could try : connect nrst to st-link also,
and set reset mode : hardware reset ; (play with mode: normal, under reset...).
2024-05-01 11:49 PM - edited 2024-05-01 11:49 PM
You're right, I didn't catch that. I was looking at "Board: --".
I finally got it to work. I had my red wire connected to VDD (pin 19 on STLinkV2). I put it on VAPP (pin 1 on STLinkV2) and it worked. But I still have to supply 3V3. But I can just use another wire and go from STLink VDD to STM32 VDD. This way I dont have to use my lab-psu.
Thank you for your help!