2024-03-01 05:11 PM
Hi all, new to this. I am trying to remove read and write protection. In the option bytes, I cannot change wrp-0 and wrp-1. The progress bar on the lower part of the gui says 100% but does not actually finish. when I check the live update box, I get a read failed message. Thanks in advance.
2024-03-03 05:01 AM
What chip is this?
> I am trying to remove read and write protection. In the option bytes, I cannot change wrp-0 and wrp-1.
What are you changing them from, and to? Perhaps change write protection on its own. RDP requires a full chip erase in some cases.
Screenshots of the error message are helpful.
2024-03-03 02:07 PM
Thank you! I was erasing older bootloader and installing a new one. I got it figured out though. I just downgraded the cube programmer to an older version and it worked.