2024-10-02 1:45 AM
Hi,
I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does it have to be connected to a PC that has STM32CubeProgrammer? Either via SSH or something similar.
Best regards and thanks in advance.
2024-10-05 12:26 AM - edited 2024-10-05 12:31 AM
@mikel-mehall wrote:Hi,
I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does it have to be connected to a PC that has STM32CubeProgrammer? Either via SSH or something similar.
Best regards and thanks in advance.
To install the SFI file remotely on your NUCLEO-U575ZI-Q, you typically need a method to flash the firmware without being directly connected to a PC running STM32CubeProgrammer. While STM32CubeProgrammer is primarily designed for local installations. Hope! it would be helpful.