cancel
Showing results for 
Search instead for 
Did you mean: 

I am working on a STM 32 project in which at debugging step I found error thatis Error: The download command you trying to perform (--download) is missing the filePath to be loaded or it has a wrong extension Error in STM32CubeProgrammer Shutting down

SGoel.2
Associate III
 
10 REPLIES 10
SGoel.2
Associate III

@MM..1​  and @Semer CHERNI​ Thank you for your help. Now I have resolve the issue it is because of the special character(&) is present in the directory path of the workspace So due to this program is not debugging Now i have changed the directory for workspace.

Hope it will helpful for others.