cancel
Showing results for 
Search instead for 
Did you mean: 

How to use STM32CubeProgrammer on a Mac?

EHans.1
Associate

I want to download a DFU file to a target using STM32CubeProgrammer (2.9.0) running on the MacOS. I can connect to the target and read its memory contents OK, but when I try to open a DFU file, the filename is grayed-out. The manual does not mention a separate driver (like there is for Windows). Help? Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
DYenEmbedded
Associate III

There was not an installer for aarch64 Mac M1

although STM32CubeIDE does run on Mac M1 and generated a .hex file, looking for a way to download to target using ST-Link/V2 or other. Anybody using Mac M1 found a way to do it ?

SetupSTM32CubeProgrammer-2_9_0_macos: Mach-O 64-bit executable x86_64

Has anybody tried to install on Parallels Virtual Ubuntu 20.04, then can it use ST-Link/V2 on Mac M1 ?

Houda GHABRI
ST Employee

Hi @EHans.1​ ,

The DFU file are not supported by STM32CubeProgrammer .

DFU file are supported only in Windows by Dfuse tool.

Houda