2019-12-06 06:49 AM
I have installed STM32CubeProgrammer V2.2.1 (https://www.st.com/en/development-tools/stm32cubeprog.html) on my MacBook without problems.
When I try to run the application, the programmer icon appears in the dock for about half a second and disappears immediately.
So I tried to open the application via terminal:
Last login: Fri Dec 6 15:40:05 on ttys000
➜ ~ /Library/Internet\ Plug-Ins/JavaAppletPlugin.plugin/Contents/Home/bin/java -version
java version "1.8.0_221"
Java(TM) SE Runtime Environment (build 1.8.0_221-b11)
Java HotSpot(TM) 64-Bit Server VM (build 25.221-b11, mixed mode)
➜ ~ java -version
java version "13.0.1" 2019-10-15
Java(TM) SE Runtime Environment (build 13.0.1+9)
Java HotSpot(TM) 64-Bit Server VM (build 13.0.1+9, mixed mode, sharing)
➜ ~ sudo open /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app
Password:
LSOpenURLsWithRole() failed with error -10810 for the file /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app.
And I can see error code -10810...
What can I do now?
Best regards!
Solved! Go to Solution.
2022-10-05 04:08 AM
I confirm this still works getting STM32CubeProgrammer working on MacOS Monterey. Thank you to everyone who has posted on this thread.