cancel
Showing results for 
Search instead for 
Did you mean: 

How to Install STM32MPU-Ecosystem-v5.1.0 Developer and Distribution packages on Windows

Carson
Associate

Hello, 

 

I am currently working on bringing up a STM32MP257F-EV1 Development board and I am having troubles. I am working on getting the STM32MPU-Ecosystem-v5.1.0 working so that I can start working on the board with Cube Programmer but all the online resources on how to get that installed are done through Linux and I am operating off windows. Is there anywhere where I can just do 1 install like for the starter-package? Or if not is there anywhere where there are Windows instructions? Any help would be so greatly appreciated.

 

Thanks!

Carson Kirk 

0 REPLIES 0