2021-12-28 9:38 PM
Hi everyone,
I'm writing my own bootloader for STM32f407VG, in the start address of flash memory. But getting problem GetID command is not acknowledged. I've attached a log also.
10:49:19:443 : RTS low
10:49:19:443 : DTR low
10:49:19:443 : Serial Port ttyUSB1 is successfully opened.
10:49:19:444 : Port configuration: parity = none, baudrate = 9600, data-bit = 8, stop-bit = 1.0, flow-control = off
10:49:19:444 : No Init bits value is : 0
10:49:19:444 : Sending init command:
10:49:19:444 : byte 0x7F sent successfully to target
10:49:19:461 : Wait ends after 1 loop, dataready = 1, delay = 9
10:49:19:461 : Received response from target: 0x79
10:49:19:462 : Activating device: OK
10:49:19:462 : Board : --
10:49:19:462 : Sending GetID command and its XOR:
10:49:19:463 : byte 0x02 sent successfully to target
10:49:19:463 : byte 0xFD sent successfully to target
10:49:19:475 : Wait ends after 1 loop, dataready = 1, delay = 6
10:49:19:475 : Received response from target: 0x79
10:49:19:483 : Received 4 data bytes from target : 0x01041379
10:49:19:483 : Chip ID: 0x413
10:49:19:483 : Sending Get command and its XOR:
10:49:19:483 : byte 0x00 sent successfully to target
10:49:19:483 : byte 0xFF sent successfully to target
10:49:19:498 : Wait ends after 1 loop, dataready = 1, delay = 16
10:49:19:498 : Received response from target: 0x79
10:49:19:498 : Received 1 data bytes from target : 0x0b
10:49:19:498 : size of bytes in the response: 11
10:49:19:514 : Received 13 data bytes from target
10:49:19:514 : Full received response: 0b31000102112131446373829279
10:49:19:514 : BootLoader protocol version: 3.1
10:49:19:515 : byte 0x11 sent successfully to target
10:49:19:515 : byte 0xEE sent successfully to target
10:49:19:614 : data sent successfully to target: 0x0800000008
10:49:19:628 : byte 0x00 sent successfully to target
10:49:19:629 : byte 0xFF sent successfully to target
10:49:19:642 : Device Read Unprotect requested
10:49:19:642 : Received 1 data bytes from target : 0x00
10:49:19:642 : Received 1 data bytes from target : 0x00
10:49:19:642 : Received 1 data bytes from target : 0x91
10:49:19:643 : Sending read unprotect command and its XOR:
10:49:19:643 : byte 0x92 sent successfully to target
10:49:19:643 : byte 0x6D sent successfully to target
10:49:19:658 : Wait ends after 1 loop, dataready = 1, delay = 15
10:49:19:659 : Received response from target: 0x79
10:49:19:659 : Received response from target: 0x79
10:49:19:665 : Sending init command:
10:49:19:665 : byte 0x7F sent successfully to target
10:49:20:649 : Wait ends after 1 loop, dataready = 1, delay = 986
10:49:20:650 : Received response from target: 0x79
10:49:20:664 : Reconnection after RDU OK !
10:49:20:664 : Checking access to flash after RDU !
10:49:20:664 : byte 0x11 sent successfully to target
10:49:20:664 : byte 0xEE sent successfully to target
10:49:20:760 : data sent successfully to target: 0x0800000008
10:49:20:782 : byte 0x00 sent successfully to target
10:49:20:782 : byte 0xFF sent successfully to target
10:49:20:796 : Sending GetID command and its XOR:
10:49:20:796 : byte 0x02 sent successfully to target
10:49:20:796 : byte 0xFD sent successfully to target
10:49:20:797 : Received response from target: 0x00
10:49:20:797 : Error: GETID command not acknowledged!
10:49:20:797 : Reemission of GetID command
10:49:20:797 : Sending GetID command and its XOR:
10:49:20:797 : byte 0x02 sent successfully to target
10:49:20:797 : byte 0xFD sent successfully to target
10:49:20:797 : Received response from target: 0x00
10:49:20:797 : Error: GETID command not acknowledged!
10:49:20:797 : Reemission of GetID command
10:49:20:798 : Sending GetID command and its XOR:
10:49:20:798 : byte 0x02 sent successfully to target
10:49:20:798 : byte 0xFD sent successfully to target
10:49:20:798 : Received response from target: 0x91
10:49:20:798 : Error: GETID command not acknowledged!
10:49:20:798 : byte 0x11 sent successfully to target
10:49:20:798 : byte 0xEE sent successfully to target
10:49:20:894 : data sent successfully to target: 0x0800000008
10:49:20:905 : UART PORT CLOSE
10:49:20:976 : Disconnected from device.
10:49:20:979 : RTS low
10:49:20:979 : DTR low
10:49:20:979 : Serial Port ttyUSB1 is successfully opened.
10:49:20:979 : Port configuration: parity = none, baudrate = 9600, data-bit = 8, stop-bit = 1.0, flow-control = off
10:49:20:979 : No Init bits value is : 0
10:49:20:979 : Sending init command:
10:49:20:979 : byte 0x7F sent successfully to target
10:49:20:985 : Wait ends after 1 loop, dataready = 1, delay = 7
10:49:20:985 : Received response from target: 0x79
10:49:20:995 : Activating device: OK
10:49:20:995 : Board : --
10:49:20:995 : Sending GetID command and its XOR:
10:49:20:995 : byte 0x02 sent successfully to target
10:49:20:996 : byte 0xFD sent successfully to target
10:49:21:001 : Wait ends after 1 loop, dataready = 1, delay = 6
10:49:21:001 : Received response from target: 0x79
10:49:21:017 : Received 4 data bytes from target : 0x01041379
10:49:21:017 : Chip ID: 0x413
10:49:21:017 : Sending Get command and its XOR:
10:49:21:017 : byte 0x00 sent successfully to target
10:49:21:017 : byte 0xFF sent successfully to target
10:49:21:033 : Wait ends after 1 loop, dataready = 1, delay = 16
10:49:21:033 : Received response from target: 0x79
10:49:21:033 : Received 1 data bytes from target : 0x0b
10:49:21:033 : size of bytes in the response: 11
10:49:21:049 : Received 13 data bytes from target
10:49:21:049 : Full received response: 0b31000102112131446373829279
10:49:21:049 : BootLoader protocol version: 3.1
10:49:21:049 : byte 0x11 sent successfully to target
10:49:21:049 : byte 0xEE sent successfully to target
10:49:21:149 : data sent successfully to target: 0x0800000008
10:49:21:171 : byte 0x00 sent successfully to target
10:49:21:171 : byte 0xFF sent successfully to target
10:49:21:189 : Device Read Unprotect requested
10:49:21:189 : Received 1 data bytes from target : 0x00
10:49:21:189 : Received 1 data bytes from target : 0x00
10:49:21:189 : Received 1 data bytes from target : 0x91
10:49:21:189 : Sending read unprotect command and its XOR:
10:49:21:190 : byte 0x92 sent successfully to target
10:49:21:190 : byte 0x6D sent successfully to target
10:49:21:203 : Wait ends after 1 loop, dataready = 1, delay = 16
10:49:21:203 : Received response from target: 0x79
10:49:21:203 : Received response from target: 0x79
10:49:21:204 : Sending init command:
10:49:21:204 : byte 0x7F sent successfully to target
10:49:22:185 : Wait ends after 1 loop, dataready = 1, delay = 985
10:49:22:185 : Received response from target: 0x79
10:49:22:195 : Reconnection after RDU OK !
10:49:22:195 : Checking access to flash after RDU !
10:49:22:195 : byte 0x11 sent successfully to target
10:49:22:195 : byte 0xEE sent successfully to target
10:49:22:295 : data sent successfully to target: 0x0800000008
10:49:22:315 : byte 0x00 sent successfully to target
10:49:22:315 : byte 0xFF sent successfully to target
10:49:22:329 : Sending GetID command and its XOR:
10:49:22:329 : byte 0x02 sent successfully to target
10:49:22:329 : byte 0xFD sent successfully to target
10:49:22:329 : Received response from target: 0x00
10:49:22:329 : Error: GETID command not acknowledged!
10:49:22:329 : Reemission of GetID command
10:49:22:329 : Sending GetID command and its XOR:
10:49:22:330 : byte 0x02 sent successfully to target
10:49:22:330 : byte 0xFD sent successfully to target
10:49:22:330 : Received response from target: 0x00
10:49:22:330 : Error: GETID command not acknowledged!
10:49:22:330 : Reemission of GetID command
10:49:22:330 : Sending GetID command and its XOR:
10:49:22:330 : byte 0x02 sent successfully to target
10:49:22:330 : byte 0xFD sent successfully to target
10:49:22:330 : Received response from target: 0x91
10:49:22:330 : Error: GETID command not acknowledged!
10:49:22:330 : byte 0x11 sent successfully to target
10:49:22:330 : byte 0xEE sent successfully to target
10:49:22:429 : data sent successfully to target: 0x0800000008I'm receiving the GetID command and sending the response as below.
uint8_t id_size = 0x01;
uart_write(ACK_BYTE);
uart_write(id_size);
uart_write(DEVICE_ID_MSB);
uart_write(DEVICE_ID_LSB);
uart_write(ACK_BYTE);
Solved! Go to Solution.
2021-12-29 3:02 AM
I think I've figured out the problem, this was happening because I've not written the read memory execution carefully. After correcting this problem now it's working.
2021-12-28 10:26 PM
Seems your code isnt executed, what debug stop? , is code on github?
2021-12-29 2:43 AM
I've debug it, it's going inside that function and other data is passing.
2021-12-29 3:02 AM
I think I've figured out the problem, this was happening because I've not written the read memory execution carefully. After correcting this problem now it's working.
2021-12-29 3:19 AM
Ok and is your code based on an open source?
2022-01-19 9:01 PM
Yes, OpenBL.