2023-03-31 6:59 AM
Hi,
I am currently asking help to flash the BLE module of my card. I think I have two problems.
The first one is hardware. I tried to connect CN5 with STLink V3mini. I think that the connection of wires is correct. And then, when I plug my STM32 and my STLink on my laptop and I try to connect my card through STM32CubeProgrammer, I get an error : STM32 target not found.
When I connect two USB devices, my laptop is not able to get connected to STM32.
So, this is my first problem.
And the second is that on STM32CubeProgrammer, I don't have the field "Firmware Upgrade Service" available, while I have the version 2.12.0...
Does someaone have an idea to upgrade the firmware, because I tried to do it in the field "Erasing & Programming" but it didn't work...
If someone could help me, or think about getting an issue, I will appreciate so much !!
2023-04-14 7:45 AM
Hello @TBarn.3 and welcome to the community,
Is it possible to check if your laptop has successfully detected the STLINK-V3MINI and allocated a port number after plugging it in?
Mohamed Aymen