cancel
Showing results for 
Search instead for 
Did you mean: 

CubeProgrammer with J-Link

DSchä.2
Associate

Is it planned that in the future the cube programmer will also work with the j-link like the cubeIDE?

5 REPLIES 5
Pavel A.
Evangelist III

+1

We have one board that cannot work with ST-LINK because of design defect (to be fixed later);

It works with J-LINK in JTAG mode.

CubeIDE can use J-LINK for loading and debugging the program but I really miss full CubeProgrammer functionality - option bytes etc, that is hard with J-LINK software.

Houda GHABRI
ST Employee

Hi @DS.5chäfer​ ,@Pavel A.​ ​ 

I see your point and will bring it up to the STM32CubeProgrammer team but to be honest it won't be treated in short term.

 Internal ticket number:  126303 (PS: This is an internal tracking number and is not accessible or usable by customers). 

Houda

Oh my gosh! I'd LOVE to use my J-Trace Pro with the STM32CubeProgrammer software.

Hi Pavel,

 

Can you please look into the following link. STM32CubeProgrammer & STM32CubeMonitor support SEGGER's J-Links

And please let me know which version of the cube programmer. 

 

kind regards,

Abdul

 

V2.16.0 can do, see:

Which cube programmer version support jlink - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".