2020-11-22 11:20 AM
i am getting the same error with cube programmer version 2.5.0
i am using windows 7 32 bit.
Java JRE build 1.8.0_271-b09
i have tried all the solutions given in previous posts but couldnt get past this.
the user manual of cube programmer 2.6.0 says :
"There is no need to install any Java™ SE Run Time Environment since version 2.6.0. The
STM32CubeProgrammer runs with a bundled JRE available inside the downloaded
package and no longer with the one installed on your machine."
please help
2020-12-10 12:27 AM
Hi @MBhar.2 ,
As your windows is 32 bit ,can you please verify that STM32CubeProgrammer 2.6.0 downloaded installed is 32bit version also?
Houda
2020-12-10 11:45 AM
Hi @Houda GHABRI
thank you for the reply.
yes i believe i have the 32 bit version.
i have the zip file
en.stm32cubeprg-win32_v2-6-0.zip
and setup file name is mentioned as
SetupSTM32CubeProgrammer_win32.exe