cancel
Showing results for 
Search instead for 
Did you mean: 

Could STM32CubeProgrammer support JTAG Chain to program several MCUs?

JieShen_Jason
Associate II

Hi,

There are four STM32 MCU on my board. I want to use one JTAG chain to cascade them. So, 

Could STM32CubeProgrammer software with J-link or ST-link simulator support JTAG Chain to program several STM32 MCU on the one Chain?

 

Thanks in advance!

Best regards!

Jason

5 REPLIES 5
JieShen_Jason
Associate II

Hi,

Any response is welcome!

Thanks in advance!

 

Best regards!

Jason

TDK
Super User

I don't think any ST tools support JTAG chaining.

 

It looks like Segger J-Link supports this if you want to use their tools instead:

Manual setup of JTAG chain - SEGGER Knowledge Base

UM08001 J-Link / J-Trace User Guide - SEGGER Knowledge Base

If you feel a post has answered your question, please click "Accept as Solution".

Hi,

Thanks!

Which software could work with Segger J-Link to  program several STM32 MCU on the one Jtag  Chain, STM32CubeProgrammer or Keil uVision5?

 

Thanks in advance!

Best regards!

Jason

 

Chris21
Senior III

Segger supplies software for their J-Link.

Debugger pane in Keil should permit you to observe devices in the JTAG chain and select which device you want to talk too.

I've not spent a lot of time with such systems, so I'd suggest you read the materials @TDK

pointed too, and perhaps bread-board an example so you're comfortable with the implementation details before committing to a PCB. Provide yourself options to break the chain so you don't build something you can't program and debug later..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..