2019-09-07 02:36 AM
hi
i am trying to make a .stldr file to be able to external load the flash ic ,
the mcu is 32f746ng and the flash is MX25L51245G , i tried to take one of the examples that provide with stmprogramer and change it to my configure , but unfortally i didnt get succes (not even a blinking led ) ,
-so i wanted to know does anyone have some example project for this spsific mcu? (the provided example are for 32L ,maybe i dont doing right the transformaition).
-is there a recommended project example that maybe will be more easy to make the changes and implent?
(attached scheme)
Solved! Go to Solution.
2019-09-07 08:24 PM
Outputs diagnostic to USART1 @ 115200 baud
2019-09-07 08:24 PM
Outputs diagnostic to USART1 @ 115200 baud
2019-09-08 01:21 AM
hi Clive thank you very much , i tried to program my app with the st-link utility and your stldr , but i get fault there , so i tried to use stmprogrammer and its start to program and succeed the program ,
but the application didn't run after reset so i plug the board off and on and then i got my blinking led but i couldn't see the nothing on my screen..
im using the flash for picture, text and fonts for the touchgfx
i didn't understand what do you mean in Outputs diagnostic to USART1 @ 115200 baud ,
so i tried to connect uart (im using stlink jtag usually) and try to program with stmprogrammer ,in this way it does't recognize the flash
so i wonder why does it program in the stmprogrammer and in st-link utility dont ,
what im doing wrong or maybe i didn't explain my self right and this stldr file have more uses...
2019-09-08 07:18 AM
STs tools are inconsistent and poorly tested.
The v2.1.0 Cube Programmer for instance doesn't call Init() before it touches memory with a read. It also won't use the Read() function if provided. It makes assumptions about memory based on MCU and address space.
The USART provides for out-of-band testing, something ST hasn't done very well.
2019-09-09 07:12 AM
Thanks so much clive, I was finally able to run and program properly, the problem was that after I went through hardware I forgot to update my memory component
now everything is working good 🙂