cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.12.0 released

Semer CHERNI
ST Employee

We are pleased to announce you that the official release of STM32CubeMX V6.12.0 is available.

  • What is new in STM32CubeMX V6.12.0?
    • New MCUs/MPUs series : STM32WB0 ,STM32MP25XX and STM32C071XX
    • Add support new CPNs STM32G4: Add support STM32G4 'Z’ and STM32G414
    • New Boards are supported: NUCLEO-C071RB , NUCLEO-WB09KE ,NUCLEO-WB07CC ,NUCLEO-WB05KZ ,STM32MP257F-DK , STM32MP257F-EV1
    • Remove STM32MP15 obsolete boards from CubeMX board selector  (  STM32MP157A-DK1 , STM32MP157A-EV1, STM32MP157C-DK2,   STM32MP157C-EV1)
    • New Boards are supported by the Start from Board feature: Nucleo-WB09xx Nucleo-WB07xx ,Nucleo-WB05xx ,Nucleo-C0 , NUCLEO-G431RB ,NUCLEO-G474RE ,NUCLEO-G491RE ,NUCLEO-H503RB ,NUCLEO-U545RE ,NUCLEO-WB15CC ,NUCLEO-WB55RG ,P-NUCLEO-WB55 ,P-NUCLEO-WB55 ,NUCLEO-WL55JC1 ,NUCLEO-WL55JC2 ,NUCLEO-WBA52CG ,NUCLEO-WBA55CG
    • Add CMake support for multicontext projects (Multi-Context ,Trust zone , Multi-core)
    • Add the support of the memory management tool for STM32WB0X and H7SC microcontrollers
    • Updated STM32CubeMX management of option bytes: STM32CubeMX preserves option bytes when regenerating a project  (H7RS ,H5, U0, WBA)
    • Add support feature (Resource Isolation Framework )RIF  / RIF Aware Ips for STM32MP25
    • LPBAM : Add missing ADF1 configuration in the LPBAM function Toolbox 
    • Add support Makefile support for WB09/07/05 and H7RS
  • Main fixed issues:
    • 164664: An issue with GUI display in STM32CubeMX.
    • 166529: TRACESWO is linked to only to Arm® Cortex®-M7 for the dual-core microcontrollers in the STM32H7 series excluding the STM32H7Rx/7Sx microcontrollers.
    • 177884: Unable to uncheck the option "save power of non-active UCPD - deactive Dead Battery pull-up" for the STM32G0 series.
    • 178050: MMC interface mode is greyed out when SDMMC1 is set to"MMC 4 bit wide bus" for the STM32H5 series.
    • 178907/179287: Incomplete generated code related to the MX_ADC3_Init() function for the STM32H7 series
    • 179275: Missing init generated code related to the MX_ADC4_Init() function for the STM32U5 series
    • 179295: Wrong generated code related to the MX_ADC1_Init() function for the STM32L4 series
    • 180281: Issue with Missing 'handle_GPDMA1' in Standard Request Mode for GPDMA Configuration for the STM32U5 series
    • 180548/181495: Oversampling ratio error for ADC3 in STM32CubeMX generated code for the SSTM32H7 series but the STM32H7Rx/7Sx microcontrollers
    • 180967: Build errors in ThreadX project with exclusive selection of LL drivers for the STM32 MCUs
    • 181386: Issue with DAC to ADC internal connection in STM32CubeMX for all the STM32H7 series but the STM32H7Rx/7Sx microcontrollers.
    • 181812: Compilation error related to the custom_stm.c file for the STM32WB series
  • Known issues fixed and problems and limitations:
    • Please refer to the wiki under this link and the release note RN0094.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0 REPLIES 0