cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.15.1 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.15.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.11.1 that is available for download.

Main issues fixed in this patch:

  • Ticket 177978 : Fixed an issue with ST-LINK firmware upgrade concerning the boards with DFU v2 or older in the version 3.14.5 of ST-LINK GDB server.
  • Ticket 178127 : Fixed an issue with the build settings: The build settings do not save the latest linker modified by the user and select the default linker instead.

Check the errata under this link for more details.

Where do I obtain STM32CubeIDE 1.15.1?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Uwe Bonnes
Chief

The download page still only offers 1.15.0.

Hey Uwe,

It'll probably take more than 56 minutes...

 

"Always be yourself. Unless you can be a pirateThen always be a pirate.”

...seems so.

AScha3_0-1714044305729.png

 

If you feel a post has answered your question, please click "Accept as Solution".