cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.15.0 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.15.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.15.0?
    • Microcontroller and board lists aligned with STM32CubeMX v6.11.0 : STM32U0, STM32H7Rx/STM32H7Sx and STM32H523/STM32H533
    • Added the support for the Q-Format in the Live Expressions view
    • Added the support for Arm® Cortex®‑A7 registers in the SFRs view
    • Switched to GCC 12 as a default toolchain
    • Added the support for Fedora® 37 and macOS 14 (Sonoma)
    • Updated to Eclipse® 2023-12
  • Main fixed issues:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Known issues fixed and problems and limitations:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Where do I obtain STM32CubeIDE 1.15.0?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0