2014-01-25 5:15 AM
Hi all,
why the LQFP32 versions of STM32F051 are not available in MicroXplorer ..??? (STM32F051KxTx) Thanks Fred #stm32cube #stm32cubemx2014-02-20 7:55 AM
Hi Fred,
I am pleased to inform you that this product is supported in STM32CubeMX.
The STM32CubeMX is part of STMicroelectronics STM32Cube™.
STM32Cube™ is an STMicroelectronics original initiative to ease developers’ life by reducing development efforts, time and cost. STM32Cube™ covers STM32 portfolio.STM32CubeMX graphical configuration tool simplifies and automates configuration and generation of STM32 initialization C code ready to be used with several development environments. The tool provides:- an easy-to-use filter for selecting the desired STM32 device and graphical wizards to simplify configuration- the pin-out wizard assists pin assignment to avoid conflicts, embedding a powerful constraints solver- the clock-tree wizard assigns clocks and performs dynamic validation- the peripherals-and-middleware wizard aids configuration to avoid unusable settings- the power-consumption wizard checks that the application meets the available power budget.The STM32CubeMX tool and STM32CubeF4 embedded software are available immediately, free of charge, directly from
.Best Regards,-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.