2024-07-16 12:11 PM
I am using STM32CubeMX 6.12.0 to generate a CMake project for VSCode on Linux. In the Software Packs Component Selector, I have chosen to include the DSP library.
STM32CubeMX includes the library and headers when generating code. So far, so good.
However, the include path, linker path and library are not specified in the the generated CMake files. I would expect these to be included by STM32CubeMX. But, not a problem. I can add them myself.
Solved! Go to Solution.
2024-07-16 03:41 PM
In case this helps anyone else, there are two steps required to use the DSP library.
To say that the requirement for the second step is a bit confusing would be an understatement. It would seem to me that enabling this component should be the default when the software pack is selected, considering it is the only option available for that component.
2024-07-16 03:41 PM
In case this helps anyone else, there are two steps required to use the DSP library.
To say that the requirement for the second step is a bit confusing would be an understatement. It would seem to me that enabling this component should be the default when the software pack is selected, considering it is the only option available for that component.