2021-09-29 1:02 AM
I cannot communicate with my computer. I detect the port but in debug mode, I see that the OTG_FS_IRQHandler interrupt is triggered regulary when I send data on my computer.
I did the same thing with my dicsovery card F411, it works. But with nucleo F756, it doesn't work. I'll give you all the parameter I set in picture linked.
To complete, when I tried to open the COM port with python, I have this error :
serial.serialutil.SerialException: Cannot configure port, something went wrong. Original message: OSError(22, 'Paramètre incorrect.', None, 87)
Do you need more details?
Could you help me? I passed a lots of time on it and I don't find.
Thank you!
2021-09-29 1:23 AM
Hello,
The fact that OTG_FS_IRQHandler is called is a good sign.
You have an example of VCP implementation in the F7 software package, so you can compare what is missing:
STM32Cube_FW_F7_V1.16.0\Projects\STM32756G_EVAL\Applications\USB_Device\CDC_Standalone
available here :
2021-09-29 6:51 AM
Thank you for your answer. I continue to search the response by comparing my code with this one
2021-09-29 9:09 AM
In fact, my program work well. It works well on windows 7 but not on windows 10, but normally, we don't need driver?
2021-09-29 9:17 AM
You don't need it, normally.
But driver is here:
2021-09-30 1:18 AM