cancel
Showing results for 
Search instead for 
Did you mean: 

USE_NEWLIB_REENTRANT

MCUpwr
Associate III

After enabling USE_NEWLIB_REENTRANT in FREERTOS (pic.1) I get error notification in LWIP (pic.2) and also after I try to compile this settings (pic3). This error info disappear when I manually put in 1 in the field
with red error text (pic.2 > RTOS Dependency).
Should there be a number 1 or some other number and is it some kind of bug? (CubeIDE Version: 1.12.1, CubeMX 6.8.1) 

1.jpg2.jpg3.jpg

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0