cancel
Showing results for 
Search instead for 
Did you mean: 

USB HS clocks not started from CubeMX 6.13 onwards

LucaP
Associate II

I am using the STM32F723 with custom, self-powered PCB interfaced to a host using USB HS. Everything worked fine with with CubeMX 6.12, but after upgrading to more recent versions, I noticed that the following functions are no longer generated within HAL_PCD_MspInit() (file usbd_conf.c):    

 

__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
__HAL_RCC_USB_OTG_HS_ULPI_CLK_ENABLE();
 
and also the corresponding clock-disabling functions in HAL_PCD_MspDeInit(). If I manually re-insert these calls, everything works again.
Anyone knows the reason why these functions are not generated, and if I am missing any USB_HS setting in more recent CubeMX versions that should be taking care of this issue? Thanks!
3 REPLIES 3
TDK
Guru

Include the IOC that you think is generating faulty code.

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hi @LucaP 

Try to reproduce with latest version V6.14 first.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


LucaP
Associate II

Hello @FBL ,

I have tried migrating the IOC from 6.12.1 to 6.13 and then to 6.14, also from 6.12.1 directly to 6.14, but in all cases those functions are no longer generated by CubeMX.

Anything else I should try?