cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to save modified .ld file when CubeMX generates the CMake project

Nobody233
Associate II

I used CubeMX to generate CMake project for STM32H750XBH6.

Nobody233_0-1720422355285.png

Then I have to modify STM32H750XBHx_FLASH.ld because DMA1 can't access the DTCMRAM.

/* Specify the memory areas */ MEMORY { DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K }
/* Uninitialized data section */ . = ALIGN(4); .bss : { /* This is used by the startup in order to initialize the .bss secion */ _sbss = .; /* define a global symbol at bss start */ __bss_start__ = _sbss; *(.bss) *(.bss*) *(COMMON) . = ALIGN(4); _ebss = .; /* define a global symbol at bss end */ __bss_end__ = _ebss; } >DTCMRAM

 But everytime I use CubeMX regenerate the project, STM32H750XBHx_FLASH.ld will be recovered. My changes didn't save.

 

How can I save this modified STM32H750XBHx_FLASH.ld when CubeMX regenerates project?

1 ACCEPTED SOLUTION

Accepted Solutions
Semer CHERNI
ST Employee

Hello @Nobody233 

First let me thank you for posting.

In fact, this is a known behavior of STM32CubeMX and under investigation. 

As a temporary solution I propose that you make modification on a back up linker file. Then use a script to copy it and replace the one imported by STM32CubeMX at each code generation.

The script could be executed using the "User action" feature in STM32CubeMX.

SemerCHERNI_0-1720531635957.png

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Semer CHERNI
ST Employee

Hello @Nobody233 

First let me thank you for posting.

In fact, this is a known behavior of STM32CubeMX and under investigation. 

As a temporary solution I propose that you make modification on a back up linker file. Then use a script to copy it and replace the one imported by STM32CubeMX at each code generation.

The script could be executed using the "User action" feature in STM32CubeMX.

SemerCHERNI_0-1720531635957.png

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

SMarie
Senior

Or, as a alternative you can create a new file STM32H750XBHx_FLASH_CUSTOM.ld with the modifications you want in it. And use this one as the linker script in your project configuration :

SMarie_1-1720533923015.png

Then on your next CubeMX generations, the STM32H750XBHx_FLASH.ld will be regenerate but not the STM32H750XBHx_FLASH_CUSTOM.ld which will still be the one used by your compiler.

 

Hi, @Semer CHERNI 

Thanks for your reply. 

Firstly, it could be work as your suggestion.

Secondly, I found another solution.

I found that "cmake\gcc-arm-none-eabi.cmake" and "CMakeLists.txt" will not be covered when CubeMX regenerates project. Then I modified this two files to use another .ld file. The STM32H750XBHx_FLASH.ld would still exist but not be used.

1. add the new .ld file.

Nobody233_1-1720579685250.png

2. add target_link_options in "CMakeLists.txt".

 

# Setup linker parameters target_link_options(${CMAKE_PROJECT_NAME} PRIVATE -T "${CMAKE_SOURCE_DIR}/STM32H750XBHx_RAM.ld" # -u _printf_float # STDIO float formatting support (remove if not used) )

 

3. remove the STM32H750XBHx_FLASH.ld in "cmake\gcc-arm-none-eabi.cmake"

 

set(CMAKE_C_LINK_FLAGS "${TARGET_FLAGS}") # set(CMAKE_C_LINK_FLAGS "${CMAKE_C_LINK_FLAGS} -T \"${CMAKE_SOURCE_DIR}/STM32H750XBHx_FLASH.ld\"") set(CMAKE_C_LINK_FLAGS "${CMAKE_C_LINK_FLAGS} --specs=nano.specs") set(CMAKE_C_LINK_FLAGS "${CMAKE_C_LINK_FLAGS} -Wl,-Map=${CMAKE_PROJECT_NAME}.map -Wl,--gc-sections") set(CMAKE_C_LINK_FLAGS "${CMAKE_C_LINK_FLAGS} -Wl,--start-group -lc -lm -Wl,--end-group") set(CMAKE_C_LINK_FLAGS "${CMAKE_C_LINK_FLAGS} -Wl,--print-memory-usage")

 

 

By the way, the 4th line of step 4 could enable the printf of float value.

 

BR,

Nobody.

Hi, @SMarie .

Thanks for your reply. 

Sorry about the point that I didn't mentioned is I'm using VS Code.

And I found another solution for VS Code, see upper floor.

 

Thanks for your kindness.

 

BR,

nobody.