cancel
Showing results for 
Search instead for 
Did you mean: 

The latest versions of CubeMx do not, on my machines, correctly generate source code for the MDK-ARM IDE. I am currently running version 6.1.1.

JCool.1
Associate II

At the end of the code generation process a message is produced that includes the text '..but MDK-ARM V5.27 project generation have a problem' (note: does this for all versions of the Keil IDE). It generates one file only; totally wrong. This behaviour occurs on: 1. Macbook Air, running High Sierra. 2. iMac running El Capitan. 3.iMac running Mojave. 4. Windows 10 running in Parallels on the Mijave iMac. However I have no problems with CubeMx v6.1.1 running on Windows 10 on a PC.

The issue appears to be related ONLY to the MDK-ARM IDE.

1 REPLY 1
Khouloud ZEMMELI
ST Employee

Hello @JCool.1​ 

Can you please provide me more details about the issue (ioc, screenshot, log file..) ?

Thanks, Khouloud