2019-04-28 8:37 AM
Dear ST,
I have problems when opening files with the .ioc extension from the previous cubemx version (5.1.0) on the latest cubemx release (5.2.0), after confirmation of installing the package needed but the file is not open but only loading forever.
Thank you for the support
2019-05-07 8:22 AM
Hey I have the same problem. This topic is marked solved. How did you solve this?
2019-05-07 7:54 PM
To solve this problem simply start "ACCESS TO MCU SELECTOR" then select the series of chips that must be loaded manually. After selecting the chip, click "Start Project" then click File -> Load Project ... Select the file with the .ioc extension that you want to open.
2019-05-09 1:58 AM
Thanks wj.anggara. It worked spot on. Weird but it works.
2019-05-09 6:55 PM
Yes. You're welcome @PGogt , happy coding :smiling_face_with_smiling_eyes: