cancel
Showing results for 
Search instead for 
Did you mean: 

testing of ublox LARA R.211 a 4G LTE with stm32f745 controller using USB_Host middleware & USB_OTG_HS ?Can anybody help with the proper CubeMX parameters or are there any CDC USB host class examples so that this module detects a virtual com port.

SG.4
Associate II

If any examples on such please if anybody finds or could share some of their experience would be of great help.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Community member​ ,

We provide some CDC USB host examples under our F7 Firmware Package.

Take a look at the example provided under the following path :

Firmware\Projects\STM32746G-Discovery\Applications\USB_Host\CDC_Standalone

You can be inspired by it.

BeST Regards,

Walid

View solution in original post

3 REPLIES 3

Hello @Community member​ ,

We provide some CDC USB host examples under our F7 Firmware Package.

Take a look at the example provided under the following path :

Firmware\Projects\STM32746G-Discovery\Applications\USB_Host\CDC_Standalone

You can be inspired by it.

BeST Regards,

Walid

Hi @Walid ZRELLI​ ,

Thank you for the fastest response.

Its of great help indeed .

Thanks a lot again.

..

Hope you have a good day . Take Care.

Regards

--

Shweta

Glad to help you :smiling_face_with_smiling_eyes: You are welcome at any time.