2024-05-13 7:49 PM
Hello engineers, I am working on a GUI interface with touchgfx. After a long period of exploration, I am now able to burn the official touchgfx sample to the development board, and now I am running into a few new problems.
Question 1: I have burned the official simple example: The Button Example shows how to handle clicks of a Button using interactions. It also shows how to interact with the nresenter A bit of logic to enable and disable buttons is done by the presenter. Through this example, I want to click the button to send data and cooperate with mobdus devices to achieve serial communication function. However, the difficulty is that I do not know how to configure usart/uart serial port through STM32cubeMX to achieve serial communication function with mobdus devices. RS232 or RS485 serial port is not found in the development board.
Question 2: Is the fan-out board (MB1280) used? If so, how should I use it? If you can use it, please give me some related circuit diagrams and use tutorials
Thank you very much!
2024-05-15 7:57 AM
Hello,
Modbus needs a library/stack to add in your application. It's not something it could be configured natively in CubeMx.
See this thread: https://community.st.com/t5/stm32-mcus-products/stm32-modbus/td-p/384413
For STM32H747-DISCO usage you can refer to its user manual on this link.and its schematics on this link.
2024-05-15 8:02 AM
Your Tutor should be providing the Tutorials.. The web is also full of material, a Google or YouTube search away.
RS232 / RS485 will need to be achieved via suitable level shifters / interface converters to get from the 3.3V CMOS signally used by the MCU.
See parts like MAX3232 / ST3232C https://www.st.com/en/interfaces-and-transceivers/st3232c.html