cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7/CubeMX bug with ADC3 and LL when using VREF/TEMP

Wolfgang Pupp
Associate III

When configuring ADC3 for VREF and/or TEMP acquisition then the necessary call to

LL_ADC_SetCommonPathInternalCh(ADC3_COMMON, LL_ADC_PATH_INTERNAL_TEMPSENSOR | LL_ADC_PATH_INTERNAL_VREFINT);

is not made. This is necessary for those channels to function correctly.

Workaround:

Call the internal path configuration function manually, followed by the proper delay before starting the ADC.

Affected (also all older version AFAIK):

STMCubeMX: 6.3.0

STMCubeIDE: 1.7.0

Both using STM32Cube FW_H7 V1.9.0

Occured with: STM32H730VBH (TFBGA100 Package)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud ZEMMELI
ST Employee

Hi @Wolfgang Pupp​ ,

I have checked from my side, and I confirm the issue, you're right.

Thanks for raising this problem to our attention and sorry for any inconvenience that may have caused, issue will be fixed.

Khouloud

View solution in original post

2 REPLIES 2
Khouloud ZEMMELI
ST Employee

Hello @Wolfgang Pupp​ ,

Thank you for your post,

I'll check it then I'll get back to you.

Khouloud

Khouloud ZEMMELI
ST Employee

Hi @Wolfgang Pupp​ ,

I have checked from my side, and I confirm the issue, you're right.

Thanks for raising this problem to our attention and sorry for any inconvenience that may have caused, issue will be fixed.

Khouloud