2022-02-02 3:43 AM
I select tim1 for sys source in STM32CubeMX and generate code.
I use STM32CubeMX V6.4.0.
I added a stripped example of the code that crashes. HAL_NVIC_EnableIRQ crashes.
Solved! Go to Solution.
2022-02-02 10:07 AM
> Break at address "0x1fff4ec0" with no debug information available,
At a glance, sounds like you've been hit with this issue:
Systick IRQ is firing, but jumping to an invalid location.
In other words, "working as intended" as far as ST is concerned.
If that is the issue, there are many threads like this.
2022-02-02 6:44 AM
Probably getting caught on the the invalid priority bug when using a non-systick time source.
https://community.st.com/s/question/0D53W00001Az92mSAB/why-assertfailed-in-halinittick
2022-02-02 7:26 AM
Code does crash at HAL_NVIC_EnableIRQ or HAL_NVIC_SetPriority if I step over them. But if I step in these functions with F5 it doesn't always crash.
The priority is set to 15. Priority group is set to 3, meaning 3 priority bits and 1 sub priority bit.
I don't know what that means, but even setting priority to 7 or 0 makes it crash.
So how do I fix it?
Confusing is that Eclipse's Open declaration of HAL_InitTick jumps to the weak version, not the overridden function in *tim.c. But the debugger steps into the correct version obviously.
2022-02-02 7:32 AM
2022-02-02 7:51 AM
"Break at address "0x1fff4ec0" with no debug information available, or outside of program code."
Program doesn't run further. Cannot break, or sometimes cannot even stop the debugger and I have to physically disconnect USB. Even without debugger connected the program doesn't run.
I added an example in my starting post.
2022-02-02 10:07 AM
> Break at address "0x1fff4ec0" with no debug information available,
At a glance, sounds like you've been hit with this issue:
Systick IRQ is firing, but jumping to an invalid location.
In other words, "working as intended" as far as ST is concerned.
If that is the issue, there are many threads like this.
2022-02-02 10:39 AM
@TDK It works! You are a life saver! This isn't the first time you fixed my issue.
I added this line to the top of main:
int main(void)
{
/* USER CODE BEGIN 1 */
SCB->VTOR = FLASH_BASE | 0;
/* USER CODE END 1 */This explains why the problem sometimes occured, but not always. The value of this register is probably random at boot and not cleared by the processor's reset circuit or the C-RTL.
2022-02-02 11:02 AM
2022-02-02 11:23 AM
I just tested. SCB->VTOR is cleared when I enter main. It is set to 0. But that cause a crash. It needs to be set to FLASH_BASE, which is 0x8000000 in my case. If I manually set the value to 0x8000000 in the watch it works too. Now I wonder why it sometimes works...
.
2022-02-14 11:23 AM
I had more stability issues after this. Crashes and often not booting. Every time I thought I found something that fixed it I discovered later that the issue returned. A cleaner way to set the VTOR is to define USER_VECT_TAB_ADDRESS in the preprocessor area of project settings. While that did reduce the number of crashes it did not stop it.
Pulling down the boot pin also helped to some extend. There were some issues with the power supply too, but that didn't fix it either.
But the one thing that seems to really have fixed it is the BOOT_LOCK byte and the nSWBOOT byte. When comparing the Option Nytes from the devboard to our MCU I found out it has different settings. Setting BOOT_LOCK to true and nSWBOOT to false with STM32CubeProgrammer prevents crashing and will guarantee booting in my case.