2025-01-26 6:54 PM
I was checking maximum frequencies of some MCUs and noticed i can pick ADC frequency in CubeMX clock configuration up to 80MHz for TSSOP-20 STM32G030. Its maximum frequency is 64MHz.
Datasheet states it can deliver maximum 2Msps on 12 bit but with its 1.5 Sampling and 12.5 conversion cycles it reaches way higher sample rates.
I checked some of the reference manual chapters and did not noticed anything unusual, prescalers seems to accept /1 divisions as well.
I am not familiar with reference manuals. Datasheet 5.3.17 also shows 35MHz maximum frequency. What's the thing i am missing? Is it a bug on interface?
2025-01-27 5:36 AM
Hello @MKanc.1 ,
The maximum frequency of STM32G030 is 64MHz as mentioned in the Datasheet.
Which CubeMX version used?
2025-01-27 5:43 AM
I had 6.12.x something before, updated to 6.13.0 and it is still same.
Stm32CubeIDE 1.16.1 have same issue, accepting ADC frequency up to 80 MHz.
2025-01-27 7:34 AM
Hi @MKanc.1 ,
An internal ticket (ID 201535) is submitted to fix this.
Thank you for your contribution and for bringing this issue to our attention.
(PS: internal ticket ID 201535 is an internal tracking number and is not accessible or usable by customers).