cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 & STM32cubeMX

diego23
Associate
Posted on October 30, 2015 at 11:05

Hello all,

when I am using STMcubeMX I can not find the SPI6 peripheral, but according the datasheet STM32F429AIH7 has SPI1, SPI2, SPI3, SPI4, SPI5 and SPI6 .

thanks in advance.

#spi6-stm32cubemx-stm32f429
2 REPLIES 2
Amel NASRI
ST Employee
Posted on October 30, 2015 at 12:29

Hi celma.diego,

Thanks for highlighting this issue. It is reported internally.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

stm32cube-t
Senior III
Posted on November 12, 2015 at 19:10

Dear user,

The package you selected ''UFBGA169'' does not have all SPI6 signals connected, such as SPI6_SCK, which is mandatory fo any of SPI6 functional modes. That's the reason why CubeMX does not display it.

Best regards