cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8T6 + MAX30003

MGGd.1
Associate II

I'm using STM32F103C8T6 controller and I want to connect MAX30003 breakout board. Which preferences it's better to use for the best performance (STMCubeMX)? 

Can I communicate it with an SPI slave using the UART1 synchronous mode (configured with CubeMX, using the LL library)??

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
schar.11
Associate II

can u please provide code for max30003 if u finished working in that.