cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX version in the STM32CubeIDE

Richard KANG
Associate

I tried this way

  1. File >> New >> STM32 Project From STM32CubeMX .ioc File.
  2. Selected the CubeMX .ioc file
  3. Click Finish

Then, CubeIDE says below

This file has been generated with STM32CubeMX version '5.6.1'.Your current STM32CubeMX version is '5.6.0'.

Please check for update: Help > Check for Updates

I already installed CubeMX 5.6.1.

When I tried "Check for Update", there are no any old version tools.

I'm using the latest versions.

Why CubeIDE detect wrong CubeMX version?

How can I resolve it?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Cartu38 OpenDev
Lead III

Most probably you are using IDE 1.3.0. Only 1.3.1 is embedding MX 5.6.1. Have a try to update your IDE relying on Help > Check for Update (menu entry without ST's logos but Eclipse native one menu entry).

B​y the the way MX integrated version is available thru Help > About ... let's click on MX icon ....