Skip to main content
Associate
December 18, 2024
Question

STM32CubeMX v6.13.0 generates broken CMake project files for STM32U5 devices

  • December 18, 2024
  • 6 replies
  • 1747 views

Hi,

I use STM32CubeMX v6.13.0 to generate a CMake project for STM32U5 devices. While code generation the process aborts with following error message:

"The Code is successfully generated under: /home/user/projects/stm32u5_firmware Project language : C but CMakeproject generation have a problem."

 
After looking in the generated CMake files, I spot various template artifacts:
 

 

cmake_minimum_required(VERSION 3.22)

project(stm32cubemx)
add_library(stm32cubemx INTERFACE)

{{sr:Enable_CMake_lanuages}}

target_compile_definitions(stm32cubemx INTERFACE{{sr:symbols_c_SYMB}}
 $<$<CONFIG:Debug>:DEBUG>
)

target_include_directories(stm32cubemx INTERFACE{{sr:include_c_DIRS}}
)

target_sources(stm32cubemx INTERFACE{{sr:sources_SRCS}}
)

target_link_directories(stm32cubemx INTERFACE{{sr:link_DIRS}}
)

target_link_libraries(stm32cubemx INTERFACE{{sr:link_LIBS}}
)

# Validate that STM32CubeMX code is compatible with C standard
if(CMAKE_C_STANDARD LESS 11)
 message(ERROR "Generated code requires C11 or higher")
endif()

{{sr:Verify_CPP_STD}}

 

Using another controller (e.g. STM32F407) everything works fine. Any idea?

Best regards,

Ben

This topic has been closed for replies.

6 replies

ST Technical Moderator
December 19, 2024

Hello @BFueldner ,

Thank you for bringing this issue to our attention!

Could you please attach your log file for further investigation of the issue?

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
BFueldnerAuthor
Associate
December 19, 2024

Hi @Souhaib MAZHOUD,

how does STM32CubeMX generate log files? The only output in the bottom of the window is:

 

Loading: /home/user/STM32CubeMX/db/plugins/boardmanager/boards/B55_Nucleo_NUCLEO-U5A5ZJ-Q_STM32U5A5ZJ_Board.ioc project
Initializing: STM32U5A5ZJTxQ

 

See attached the IOC and the CMakeLists.txt. For me it seems that the CMakeProject template did not get the right files to solve the placeholders. In the .mxproject file (renamed in attachment to mxproject.txt) all needed files are listet.

Best regards,

Ben

ST Technical Moderator
December 20, 2024

Hello @BFueldner 

Thank you for your clarification.
This issue has been raised to the relevant team, and it is tracked by internal ticket 199074.

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
BFueldnerAuthor
Associate
March 5, 2025

The new STM32CubeMX release 6.14.0 is out, announced with CMake improvements. But the CMake generator seems to get even worse:

cmake_minimum_required(VERSION 3.22)
{{sr:Enable_CMake_lanuages}}
# STM32CubeMX generated symbols (macros)
set(MX_Defines_Syms{{sr:symbols_c_SYMB}}
 $<$<CONFIG:Debug>:DEBUG>
)

# STM32CubeMX generated include paths
set(MX_Include_Dirs{{sr:include_c_DIRS}}
)

# STM32CubeMX generated application sources
{{sr:STM32_Application_ToReplace}}
# STM32 HAL/LL Drivers
{{sr:STM32_Drivers_ToReplace}}
# Drivers Midllewares

{{sr:drivers_midllewares}}

# Link directories setup
set(MX_LINK_DIRS
{{sr:link_DIRS}}
)
# Project static libraries
set(MX_LINK_LIBS {{sr:link_LIBS}}
 STM32_Drivers
 {{sr:list_library}}
)
# Interface library for includes and symbols
add_library(stm32cubemx INTERFACE)
target_include_directories(stm32cubemx INTERFACE ${MX_Include_Dirs})
target_compile_definitions(stm32cubemx INTERFACE ${MX_Defines_Syms})

# Create STM32_Drivers static library
add_library(STM32_Drivers OBJECT)
target_sources(STM32_Drivers PRIVATE ${STM32_Drivers_Src})
target_link_libraries(STM32_Drivers PUBLIC stm32cubemx)
{{sr:Verify_CPP_STD}}
{{sr:add_library_ToReplace}}
# Add STM32CubeMX generated application sources to the project
target_sources(${CMAKE_PROJECT_NAME} PRIVATE ${MX_Application_Src})

# Link directories setup
target_link_directories(${CMAKE_PROJECT_NAME} PRIVATE ${MX_LINK_DIRS})

# Add libraries to the project
target_link_libraries(${CMAKE_PROJECT_NAME} ${MX_LINK_LIBS})

# Add the map file to the list of files to be removed with 'clean' target
set_target_properties(${CMAKE_PROJECT_NAME} PROPERTIES ADDITIONAL_CLEAN_FILES ${CMAKE_PROJECT_NAME}.map)

# Validate that STM32CubeMX code is compatible with C standard
if((CMAKE_C_STANDARD EQUAL 90) OR (CMAKE_C_STANDARD EQUAL 99))
 message(ERROR "Generated code requires C11 or higher")
endif()

When are you planning to finally fix this problem?

Best regards

Associate II
June 18, 2025

I have exactly the same problem with the STM32U5A5AJH6Q mcu.

To reproduce this bug, simply create a new project with this MCU, change the toolchain to CMake and generate the code.


Here the error message of CubeMX:

 

Spoiler

2025-06-18 11:31:59,712 [INFO] ProjectBuilder:4912 - Project Generator version: 4.6.0.1-B1
2025-06-18 11:31:59,748 [INFO] ConfigFileManager:1590 - The Die is : DIE481
2025-06-18 11:31:59,994 [INFO] ToolchainGenerator:587 - stack trace : java.lang.reflect.InvocationTargetException
at java.base/jdk.internal.reflect.DirectMethodHandleAccessor.invoke(DirectMethodHandleAccessor.java:118)
at java.base/java.lang.reflect.Method.invoke(Method.java:580)
at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.CallMethod(ToolchainGenerator.java:406)
at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.update(ToolchainGenerator.java:577)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:5179)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:984)
at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:61)
Caused by: java.lang.StringIndexOutOfBoundsException: Range [-1, 0) out of bounds for length 0
at java.base/jdk.internal.util.Preconditions$1.apply(Preconditions.java:55)
at java.base/jdk.internal.util.Preconditions$1.apply(Preconditions.java:52)
at java.base/jdk.internal.util.Preconditions$4.apply(Preconditions.java:213)
at java.base/jdk.internal.util.Preconditions$4.apply(Preconditions.java:210)
at java.base/jdk.internal.util.Preconditions.outOfBounds(Preconditions.java:98)
at java.base/jdk.internal.util.Preconditions.outOfBoundsCheckFromToIndex(Preconditions.java:112)
at java.base/jdk.internal.util.Preconditions.checkFromToIndex(Preconditions.java:349)
at java.base/java.lang.String.checkBoundsBeginEnd(String.java:4865)
at java.base/java.lang.String.substring(String.java:2834)
at java.base/java.lang.String.substring(String.java:2807)
at generators.CMakeGenerator.generateCMake(CMakeGenerator.java:358)
at convertor.Convertor.generateMakefileProject(Convertor.java:3123)
at convertor.Convertor.generateCMake(Convertor.java:2952)
at convertor.Convertor.generate(Convertor.java:740)
at convertor.Convertor.convert(Convertor.java:553)
at convertor.Convertor.updateProject(Convertor.java:430)
at java.base/jdk.internal.reflect.DirectMethodHandleAccessor.invoke(DirectMethodHandleAccessor.java:103)
... 6 more

2025-06-18 11:31:59,994 [INFO] ToolchainGenerator:588 - [Project Generator] Problem in the update of the project
2025-06-18 11:31:59,995 [INFO] ConfigFileManager:3123 - mx.scratch is deleted!

 

 

Peter Allnutt
Associate III
July 3, 2025

Was having the same problem using STM32CubeMX 6.14.1 and have found this topic. I then tried a project for the  STM32WL55J1 Nucleo board. I didn't get the same 

 

"The Code is successfully generated under: /home/user/projects/stm32u5_firmware Project language : C but CMakeproject generation have a problem."

error that I get with the U5A board but the resultant cmake files are as screwed up with numerous {{sr:blah blah}} errors

 

I've just tried a project for the STM323240G-EVAL board so not everything it broken.