2024-07-08 8:21 AM
When i try to set ADC sequencer to not fully configurable, ADC shows ADC_Regular_conversion_Mode error after migration of the .ioc file from previous version of CubeMx. In the previous version of CubeMx everything worked well. Help please!
Solved! Go to Solution.
2024-07-08 8:23 AM - edited 2024-09-24 12:16 PM
Hello @Tibor_effman and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This is a Known issue reported on this post and escalated internally for correction. Thank you so much for reporting.
Update: This issue has been solved on the V6.12.1 of CubeMX.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-08 8:23 AM - edited 2024-09-24 12:16 PM
Hello @Tibor_effman and welcome to the ST Community :smiling_face_with_smiling_eyes:.
This is a Known issue reported on this post and escalated internally for correction. Thank you so much for reporting.
Update: This issue has been solved on the V6.12.1 of CubeMX.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-05 6:16 PM
Hello,
I am having the exact issue. When is the patch expected to download? Meantime, Is there any workaround?
Thanks,
2024-09-24 10:57 AM - edited 2024-09-24 11:19 AM
Hello
The issue is solved in 1.16.1.
Thanks