cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX V4.21.0 and Java 1.8.0_131 crash

Vu TRAN
Associate II
Posted on June 20, 2017 at 17:49

Since my last update of WIN10, Java and STM32CubeMX (I did all after Windows update) my STM32 Cube MX crashed on lot of actions : can not load a project, can not save project etc... Any suggestion ?

My PC runs WIN10 64bit

#java8 #cubemx-4.21
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee
Posted on June 21, 2017 at 11:13

Hi

TRAN.Vu

,

Thank you for your reported issue.

This is known issue in CubeMX with Windows 10/Java 8 and it is under investigation by ourteam.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Ralph E
Associate II
Posted on June 24, 2017 at 16:35

Hi,

if you first create a 'Project name' in 'Generate Project report files' or 'Generate source code..' the saving with 'CTRL+S' works without crash.

'Load Project' CTRL+L  doesn't work. I used 'Recent projects'

It's only a workaround. ST please correct the bug. (;-)

Regards

Ralph

PS: WIN10 Pro - 64Bit, Java 1.8.0_131 x86_64, STM32CubeMX 4.21.0

Posted on June 25, 2017 at 16:01

Hi Ralph, Thank For your advice, I cam at least continue working with this tip.

Reagrds

Ralph E
Associate II
Posted on July 15, 2017 at 15:33

Try this 

Remove Windows 10 'GodMode shortcut'

Thanks to: 

https://stackoverflow.com/questions/43836174/java-applications-crash-when-browse-control-used

 

After erase, it work's

RDE

Posted on July 18, 2017 at 16:27

Hi Ralph, I confirm efficiency of your tip... Many thanks.

Cheer