2016-12-15 06:31 AM
I'm using using STM32cubeMX to generate the init code for an STM32373C-EVAL board and have found this problem setting up the SDADC (see picture).
Basically, I can't set 'Configuration index' to anything other than the default which it tells me is not valid.
If I ignore all the error messages and generate the code anyway, it does actually generate good code which works.
I'm just learning this tool so thought I'd ask if I am doing anything wrong...
It's cube version 4.18 on Ubuntu linux.
Thanks !
#stm32cubemx2016-12-17 06:23 AM
Dear
legge.darren
,I will check this case, then I getback to you as soon as possible.
Thanks for sharing your feedback.
Best Regards
-Imen-
2016-12-21 08:06 AM
Thanks. I think it was actually because I had selected 'single ended' rather than 'single ended zero-reference' on the 'Pinout' tab. Then in the screen above, 'single ended zero volt reference mode' was selected (which needed to be single ended offset mode to match). Probably...
2017-05-02 07:50 AM
Hello
Legge.Darren
,Thanks for reporting this issue.
We have just fixed and it will be delivered in the next CubeMX release (4.21) that will come soon!
BR. Eric