2024-04-25 11:41 PM
Hi everyone,
I used STM32CubeMX (version 6.11.1) to generate the initialization code for an STM32G491RCT.
The toolchain is configured as a Makefile project.
At the end of the C_SOURCES definition, it specifies sysmem.c and syscalls.c.
# C sources
C_SOURCES = \
Core/Src/main.c \
...
Core/Src/sysmem.c \
Core/Src/syscalls.cHowever, those two files were not generated, resulting in the following error:
make: *** No rule to make target 'build/sysmem.o', needed by 'build/firmware.elf'. Stop.
Is this a bug in STM32CubeMX or am I supposed to implement the functions myself?
2024-04-26 12:50 AM
Hello @mbaer_zg and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I'm not able to reproduce this
Can you add more details.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-26 1:51 AM - edited 2024-04-26 1:54 AM
I tested a few configurations and I think it is a combination of "STM32Cube MCU packages and embedded software packs" setting and regenerating.
If I have a blank project (only .ioc, no files generated) and I generate the source files for the first time with "Copy only the necessary library files" selected, then the sysmem.c and syscalls.c won't be generated.
When I do the same thing (blank project, first generation) but I select "Copy all used libraries into the project folder", then the sysmem.c and syscalls.c get generated.
If I delete the two files and regenerate, the files don't get regenerated.
You can reproduce the behavior by creating a new project, selecting "Copy only the necessary library files" and generating the code.
2024-06-11 5:33 AM
I saw this issue when I migrated my makefile project from STM32CubeMX v6.11.0 to v6.11.1. My also have the "Copy Only Necessary library files" option selected.
My old project folder using v6.11.0 did not contain sysmem.c and syscalls.c files.
After the migration and subsequent regenerating the makefile now contains the extra two lines for sysmem.c and syscalls.c but the folder does not contain these files.
2024-10-17 2:04 AM
I am facing the same issue with STM32CubeMX v6.12.1
2025-02-27 3:30 AM
Using STM32CubeMX v6.13.0 and still happens this error. Whether makefile includes this files when not needed or the files are needed and not generated.
I'm able to reproduce exactly the same behaviour as described by mbaer_zg
(Note on this version: The change from v6.12.x to v6.13.0 really solved an issue with the linker script flash.ld, where RAM was missing from some places discussed here: FLASH.ld syntax error when upgrading to CubeMX v6.12.1 )