cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX ignores ''Uses FreeRTOS functions'' checkbox

Hiroshi Sakurai
Associate II
Posted on March 24, 2017 at 07:28

I'm trying to make a interrupt handler which doesn't use FreeRTOS function and preemption priority is higher than FreeRTOS, say 2.

However every time I load .ioc file, STM32CubeMX checks the 'Uses FreeRTOS functions' checkbox of the interrupt handler, so I need to uncheck it manually.

Please try with the attached .ioc file.

STM32CubeMX version is 4.20.0

STM32Cube FW_F7 V1.4.1

#stm32cubemx
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on March 24, 2017 at 13:36

Hello, 

Your issue is reported internally to our CubeMx team for further check.

You should use the last version of STM32CubeF7 firmware package which contains fix defect, enhancements and updates to new version of FreeRTOS V9.0.0

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on April 27, 2017 at 15:00

Hi

Sakurai.Hiroshi

,

For your information, the issue you reported will be delivered in the next CubeMX release (4.21).

BR. Eric